STM32H753: Cannot enter/connect to Bootloader using USART1
Hello everyone,
this is my first time building an STM32 Based Board myself.
I am trying to talk to the Chip Using a CP2102 UART Bridge connected to PA9 & 10.
For Reset and Boot 0 ive connected Reset (NRST) to RTS of the UART Bridge and Boot0 to its GPIO0 Pin and configured that Pin in the Bridge. I have however also tried just pulling Boot0 High and Jumping NRST to GND and then immediately connecting using STM32CubeProgrammer.
Using an Oscilloscope ive found that the Magic Packet is sent to the STM32 (0x7F, 115200 Baud, Even Parity, 1 Stop) but there is no response (Tx of the STM32 stays high all the Time).
PB15 is left floating, I am using the VIT6 Variant (The LQFP100 Package), its a Brand new Chip, is there any configuration required before this works?