cancel
Showing results for 
Search instead for 
Did you mean: 

Crystal oscillator selection for 170MHz | STM32G484RET

Matthew47
Associate

Hi,

I am designing a STM32G484RET into an application, and I wanted to confirm that my oscillator design will theoretically operate before having it manufactured.

Target clock speed: 170MHz

Crystal chosen: https://www.digikey.com/en/products/detail/ecs-inc/ECS-240-10-30B-CKM-TR/8023196

Closest available capacitors: https://www.digikey.com/en/products/detail/kemet/C0805C330F5GACTU/2212505

Resources used for design: AN2867

CL = (C1 * C2) / (C1 + C2) + Cstray

-Matthew

Matthew47_0-1743968317088.png

 

6 REPLIES 6
mƎALLEm
ST Employee

Hello @Matthew47 and welcome to the ST community;

As you referred to the application note AN2867, what is the calculation you did and what was the result so we could verify?

The most important thing to start with is the "Oscillator transconductance":

Read the AN2867 / section 3.4 Oscillator transconductance.

There is a calculation example provided there:

mALLEm_0-1743971767508.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi,

I used the following setup in Excel to calculate the values. I assumed C_stray to ~3pF, and then pulled the 20pF C_L from the crystal data sheet.

Matthew47_0-1743972158974.png

-Matthew

 

Before going ahead with CL what calculation you did for gm/gm_crit?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

And for the CL calculation see this thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
STOne-32
ST Employee

Dear @Matthew47 ,

I'm not sure that the part selected in the schematics has 20pF of CL ..     it should be 10pF instead as mentioned in the datasheet.  

STOne32_0-1743973333746.png

 

STOne32_1-1743973543074.png

ESR Max is 30Ohm for 24MHz and here is a Bonus from our Partner ECS :

 

STOne32_3-1743973905529.png

 

Microsoft Power BI

 

Hope it helps you

Ciao

STOne-32.

Good catch! Looks like my capacitors should be about 10pF

Matthew47_0-1743979212372.png