cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32U595 DFU work with external HSE oszillator?

Uwe Bonnes
Chief

AN2606 Figure 115." Bootloader V9.x selection for STM32U595xx/99xx/A5xx/A9xx" show  that the Bootloader USB detection aborts DFU startup to a system reset when no quarz is found. Does this abort  also happen if an external HSE oscillator is used?

2 REPLIES 2
TDK
Super User

They're the same thing. "Quartz detected" is short for "external HSE oscillator is present, working, and is a frequency supported by the DFU."

To use the USB DFU on this chip, you need to have an HSE crystal onboard.

You can find more details in the USB DFU document.

USB DFU protocol used in the STM32 bootloader - Application note

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Super User

Oh, you probably are asking about HSE in bypass mode with an external clock. It is not guaranteed to work, but it might. See workarounds here for STM32L1. Could be similar for STM32H5.

Solved: How to run USB DFU bootloader from HSE oscillator ... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".