Skip to main content
NAbun.1
Associate II
Mar 4, 2025 10:49 PM UTC
Solved

What is the actual STM32 pin capacitance (for the purpose of sizing an HSE crystal)?

Hello,

I originally tagged onto this thread: https://community.st.com/t5/stm32-mcus-products/stm32f103-hse-crystal-capacitors/td-p/771200 but I was recommended to make a separate thread.

 

Many of the STM32 datasheets, such as the STM32H753, say that the pin capacitance is 5pF per pin. When trying to size a crystal for the HSE oscillator, the designer is told to follow AN2867. When trying to calculate the stray capacitance we (at a minimum) add the pin capacitance of the two oscillator pins to get 10pF. The STM32H753 datasheet even says to approximate 10pF here on page 232:

NAbun1_0-1741128293961.png

AN2867 does not recommend any crystals for the STM32 HSE oscillator, so the assumption is that crystal has to have higher than 10pF load capacitance for STM32 devices. 

I understand that pin capacitance would vary per package. Does ST have a more accurate estimation of pin capacitance? Or does ST have recommendations for crystals for the STM32 HSE oscillator?

Thanks,

Nino

This topic has been closed for replies.
STOne-32
STOne-32Best answer
ST Technical Moderator
Mar 10, 2025 7:20 PM UTC

Dear @NAbun.1 ,

I would assume that you can start by having  Cs ( Total Cpin  and Cpcb) = 3pF .  but in the formula it will be this one

if Crystal CL=8pF ( as you purchased in datasheet of the crystal).    (CL-Cs)*2 = CL1=CL2.

(8pF-3pF)* 2 =  10pF and not 4pF for each CL1/CL2 cap leg to add.      Cs is subtracted only once and is the equivalent parallel capacitance seen by the Oscillator /crystal.

Hope it helps you.

 

Ciao

STOne-32. 

8 replies

jiangfan
ST Employee
Mar 5, 2025 9:00 AM UTC

Yes, pin capacitance will vary per package, QFP has higher pin capacitance than BGA.

from experience, I agree that "pin capacitance should be in range of 2pF to 3pF in general, in our datasheet we are providing worst case typical condition of 5pF ( generic to all I/Os)" of post:

Crystals and load capacitors for stm32l432 - STMicroelectronics Community

 

although no recommendation from ST for crystals regarding the STM32 HSE oscillator, you may try to use same HSE crystal of official STM32 board.

NAbun.1
NAbun.1Author
Associate II
Mar 5, 2025 4:43 PM UTC

Hi @jiangfan ,

Thank you for your response. In the post you linked, they are discussing a UFQFPN32 (5x5) package, which I imagine is one of the lower pin capacitance parts.

Does the 2pF to 3pF apply to the STM32H753 LQFP100 (14 x 14 mm) package, or is that more likely to see the worst case, ad we should plan for the full 5pF?

 

Thanks,

Nino

jiangfan
ST Employee
Mar 6, 2025 2:45 AM UTC

I would like to assume ~2pF for BGA/QFN, and assume ~3pF for QFP.

STOne-32
ST Technical Moderator
Mar 5, 2025 6:59 PM UTC

Dear @NAbun.1 ,

I confirm what has been communicated by @jiangfan ( our boards expert here ) :) You can assume that HSE In/out pins are in range of 2 to 3pF on your selected LQFP100 package as worst case . In fact, it is very easy to obtain it with empirical testing on your PCB. Let’s called  “Cs” which is the Sum of pads and PCB parasitic capacitance .

if you choose a crystal of 8pF CL ( crystal datasheets ) , You can start by putting on the two legs CL1 and CL2  two capacitors of  10pF - which is { 8-3}  * 2 , then output the HSE frequency  and monitor the nominal frequency using a good oscilloscope or universal counter. The right value of CL1/CL2 you can adjust is when the MCO output is the closed to the Nominal Frequency of the crystal ( written in Datasheet +/- XXPPM) then you can adjust and deduce the exact Cs of your PCB including internal pads . Try it and let us know with scopes .

if the frequency is a bit higher than nominal , you need to add extra capacitance on CL1/CL2, if it slower you need to remove and reduce 10pF to smaller value .

 

Hope it helps you,

STOne-32

NAbun.1
NAbun.1Author
Associate II
Mar 10, 2025 5:22 PM UTC

Hello @jiangfan & @STOne-32 

 

Thank you very much for your helpful replies. I apologize for my late response as I was on vacation. I have one last follow up.

I just want to clarify if the capacitance is 2-3pF per pin or 2-3pF of total stray capacitance? @STOne-32 seemed to use 3pF as the total stray capacitance in his equation, but I would think it would be (8pF - 3pF * 2) * 2 = 4pF given the two pins, but perhaps I am misunderstanding?

 

-Nino 

STOne-32
STOne-32Best answer
ST Technical Moderator
Mar 10, 2025 7:20 PM UTC

Dear @NAbun.1 ,

I would assume that you can start by having  Cs ( Total Cpin  and Cpcb) = 3pF .  but in the formula it will be this one

if Crystal CL=8pF ( as you purchased in datasheet of the crystal).    (CL-Cs)*2 = CL1=CL2.

(8pF-3pF)* 2 =  10pF and not 4pF for each CL1/CL2 cap leg to add.      Cs is subtracted only once and is the equivalent parallel capacitance seen by the Oscillator /crystal.

Hope it helps you.

 

Ciao

STOne-32. 

NAbun.1
NAbun.1Author
Associate II
Mar 19, 2025 8:12 PM UTC

Hi @STOne-32, thank you. I'll probably start with 3pF for Cpin, but might add a tiny bit more for Cpcb depending on the copper thickness or stackup. I will, of course, verify after build. I just wanted to make sure I didn't have to change the layout to accommodate a larger crystal, which it seems like I don't have to. =)

 

mƎALLEm
ST Technical Moderator
Apr 17, 2025 6:42 PM UTC

Hello,

A new article "How to select a compatible crystal and load capacitors for STM32 with layout guidelines" has been published today and this thread has been linked to that article in the "Related links" section.

Good reading.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.