2007-06-14 10:21 PM
what is wrong with the connection of Jlink and IAR workbench?
2007-06-14 03:22 PM
what may be wrong between Jlink and IAR workbench with message below?
Fri Jun 15 09:19:16 2007: J-Link firmware: V1.20 (J-Link compiled Feb 08 2006 15:44:22 ARM Rev.5) Fri Jun 15 09:19:16 2007: JTAG speed is initially set to: 4000 kHz Fri Jun 15 09:19:16 2007: Resetting Target using RESET pin Fri Jun 15 09:19:16 2007: Halting CPU core Fri Jun 15 09:19:16 2007: Initial reset was performed Fri Jun 15 09:19:16 2007: J-Link found 1 JTAG device. ARM core Id: 3F0F0F0F(ARM7) Fri Jun 15 09:19:16 2007: Device at TAP0 selected Fri Jun 15 09:19:16 2007: **** Warning: Chip has already been halted. Fri Jun 15 09:19:16 2007: Auto JTAG speed: 4000 kHz Fri Jun 15 09:19:17 2007: 4545 bytes downloaded (8.11 Kbytes/sec) Fri Jun 15 09:19:17 2007: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 4.0 Kickstart\arm\ config\flashloader\ST\FlashSTR71xF.d79 Fri Jun 15 09:19:17 2007: Target reset Fri Jun 15 09:19:36 2007: Memory access timed out @ 20000B5C Fri Jun 15 09:19:55 2007: Code still contains old breakpoints