cancel
Showing results for 
Search instead for 
Did you mean: 

what is wrong with the connection of Jlink and IAR workbench?

hg-chen
Associate II
Posted on June 15, 2007 at 07:21

what is wrong with the connection of Jlink and IAR workbench?

1 REPLY 1
hg-chen
Associate II
Posted on June 15, 2007 at 00:22

what may be wrong between Jlink and IAR workbench with message below?

Fri Jun 15 09:19:16 2007: J-Link firmware: V1.20 (J-Link compiled Feb 08 2006 15:44:22 ARM Rev.5)

Fri Jun 15 09:19:16 2007: JTAG speed is initially set to: 4000 kHz

Fri Jun 15 09:19:16 2007: Resetting Target using RESET pin

Fri Jun 15 09:19:16 2007: Halting CPU core

Fri Jun 15 09:19:16 2007: Initial reset was performed

Fri Jun 15 09:19:16 2007: J-Link found 1 JTAG device. ARM core Id: 3F0F0F0F(ARM7)

Fri Jun 15 09:19:16 2007: Device at TAP0 selected

Fri Jun 15 09:19:16 2007: **** Warning: Chip has already been halted.

Fri Jun 15 09:19:16 2007: Auto JTAG speed: 4000 kHz

Fri Jun 15 09:19:17 2007: 4545 bytes downloaded (8.11 Kbytes/sec)

Fri Jun 15 09:19:17 2007: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 4.0 Kickstart\arm\

config\flashloader\ST\FlashSTR71xF.d79

Fri Jun 15 09:19:17 2007: Target reset

Fri Jun 15 09:19:36 2007: Memory access timed out @ 20000B5C

Fri Jun 15 09:19:55 2007: Code still contains old breakpoints