cancel
Showing results for 
Search instead for 
Did you mean: 

Vnd7020 self internal diagnostic

SGasp.1
Senior

Hi community I am working with gate driver vnd7020.

I have already implemented the reading of the current (I) for both 2 oyputs and temperature for every chip

Now i want to implement the self diagnostic from the driver.

SGasp1_0-1701163555512.png

I want to detect the overload and undervoltage condition. 

What is nopt clear is what i have to expect to have from the adc reading in both the conditions ()

SGasp1_1-1701163709950.png

if i understand correctly if i read the adc in the same case as i am reading the current if i find VsenseH that means that has been the overload condintion? 

So this means that when i read the adc value from the mcu i should expect 0 or 4096 (max range for my adc)??

Another question is about how to simulate this condition in the gate driver without doing an overload.. 

Thanks a lot for the answer 

 

 

 

0 REPLIES 0