2006-10-30 3:11 AM
Unexpected end of file error during installation of arm-elf toolchain
2006-09-24 10:32 PM
Hi!
I want to start development with uClinux on a STR7 So I downloaded the Application Note 2119 from ST, ''Getting Started with uClinux for STR710''. But the first step already produces a failure. gunzip: stdin: unexpected end of file tar: Read 4903 bytes from - tar: unexpected EOF in archive tar: unexpected EOF in archive tar: error is not recoverable: exiting now You can also have a look to the attachment. I tried it in Cygwin running under Windows XP Prof., Damn Small Linux (DSL), Knoppix and at last on a Debian installation - but I get this error on every system. I even tried two different computers. What system works with the description of the application note and what version of it? Thanks for help! Michael ________________ Attachments : toolchain_error.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOF&d=%2Fa%2F0X0000000aPK%2FpeK6_IWSuXd_zD3SLnA7WCOT8rt2sf5qkqDvt7f3ggQ&asPdf=false