2024-10-17 10:56 PM
I am trying to use DWM1000 for ranging as well as communication but I am unable to do it . I debugged the code and Know that Initiator is sending data but is not being heard . The Rx buffer in responder is geting updated by random values.
I have attached the code to both here . If anyone could help it will be very helpful.
https://drive.google.com/drive/folders/16WMlzlzvSzrWMwefvTAwKB4aY1TVz7GR?usp=sharing
https://drive.google.com/drive/folders/14RmWrQQ4oUgmkux6U1B235Gc2GPwN-bo?usp=sharing
Solved! Go to Solution.
2024-10-22 11:02 PM
I tried everything . ALL I knbow as of now is that there is an issue due to timing and thus the devices are not getting connected
2024-10-23 12:38 AM
I am working with DWM 1000 and STM32f429zit and stm32g491ret which I have used and worked fine for data transmission I want to use the same for the ranging purpose . At th initiator tx_count increases continously as indication of data being transmitted on other hand at responder the rx_buffer is already full with garbage and this stops the responder for completeing the further . If anyone has worked with this in partivcular or knows a way to get rid of the issue kindly respond ASAP.
I have attached both codes to this mail.
2024-10-23 12:55 AM
@Rituraj wrote:At th initiator tx_count increases continously as indication of data being transmitted .
Again, that does not confirm that anything is actually been transmitted to the air.
Don't Qorvo provide tools to "sniff" what's actually being transmitted to air?
@Rituraj wrote:If anyone has worked with this in partivcular
The best place to find such people would be on the device manufacturer's forum:
https://forum.qorvo.com/c/wireless-connectivity/10
2024-10-23 1:06 AM
I already tried to get answers on Qorvo forum but I am getting no response at all.
A Sniff code has been provided but its for a BLE sniffer and I will need to start working on nrf sdk to utilize that.
I checked using a dummy antenna and oscilloscope . I know the wave exists and is being transmitted as I checked on DSO but again I need it to be recieved on DWM1000 module
2024-10-23 1:16 AM
So have you contacted Qorvo support?
2024-10-23 1:49 AM
yes , did that too . No response till now
2024-10-23 1:59 AM
Do you have a distributor to help?
Do you have the Qorvo dev kit?
I would strongly recommend to always start with the manufacturer's own dev kit - especially when you're unfamiliar with the part.
2024-10-23 3:05 AM
No dev kit .
I debugged it for every possible way. I know for sure that transmission is being done as I can read the SYS_ STATUS but on the responder end even this changes very rapidly and according to what I compared there is and Interrupt that is preventing operation.
2024-10-23 3:08 AM
@Rituraj wrote:No dev kit .
Again, I would strongly suggest that you get one - then you have a known-good starting point.
You are also far more likely to get support on that than on some unknown custom setup.