2004-11-02 9:07 PM
2004-10-18 3:52 AM
Hi! Does anybody knows / has an exapmle for using one of the timer as a counter without using the GPIO. Just initialize the timer, set an external variable to a specific value wich will be counted down/up by the interruptroutine. In my program, i use the timer just as a counter but
my main problem is the prescalervalue. I can change it between 0xf and 0xf0 and the time between 2 interrupts will change from 31 microseconds to 148 microsecond. This seems to be very short. I would like to have times around 10-100 milliseconds between an interrupt. So, perhaps i have something forgotten to initialize and somebody has a suggestion? hein_b void start_time1(ushort x_in_sek) { u32 sekundenfaktor=1; // 10 timer1_cnt = 0x1*sekundenfaktor*x_in_sek; // 0x300 *... Myprescaler1=0x50; // just for time-measurements (not necessary for real program) // Configure Port 2 pins GPIO_Config (GPIO0, 0xFFFF, GPIO_OUT_PP); GPIO0->PD = 0x0000; // Initialize the Timer TIM_Init ( TIM1 ); //--------------------------------------------------------------------------- // Configure the EIC Timer1 IRQ channel //--------------------------------------------------------------------------- EIC_IRQChannelConfig( T1TIMI_IRQChannel, ENABLE ); EIC_IRQChannelPriorityConfig( T1TIMI_IRQChannel , 1); EIC_IRQConfig( ENABLE ); // Configure the TIM Prescaler TIM_PrescalerConfig ( TIM1, Myprescaler1 ); // Enable the OverFlow Interrupt TIM_ITConfig ( TIM1 , TIM_TO_IT , ENABLE ); TIM_CounterConfig ( TIM1, TIM_START ); // own flags timer1_fin = 0; // ;timer ist noch nicht abgelaufen timer1_run = 1; // ;timer laeuft time_out = 0; return; } // routine, called by the interruptprogram void cnt_dwn1() { if (timer1_run==1) // und der timer laeuft { if (timer1_cnt > 0) // und noch nicht abgelaufen ist { timer1_cnt -=1; // dann einen runterzaehlen // GPIO0->PD = ~GPIO0->PD; //just for time measurement } else { time_out = 1; // sonst time_out flag setzen! } } }2004-10-28 12:58 AM
Thx for Help. Your suggestion was't the problem. Timerproblem is solved now, i had problems to understand the TIM_OCFA feature.
2004-11-01 9:39 PM
I have the same question.
Could you give me some advice?2004-11-01 10:03 PM
The overflow interrupt works properly.
But I still want to know more information about OCFA. For example: How to make a interrupt when TIMn_CNTR matches TIMnOCAR. Thanks for your help