Posted on October 28, 2004 at 09:58Thx for Help. Your suggestion was't the problem. Timerproblem is solved now, i had problems to understand the TIM_OCFA feature.
Posted on October 18, 2004 at 12:52Hi! Does anybody knows / has an exapmle for using one of the timer as a counter without using the GPIO. Just initialize the timer, set an external variable to a specific value wich will be counted down/up by the in...
Posted on September 27, 2004 at 14:39Quote:On 2004-07-27 10:20, RISC wrote: In your source files replace the str71xDL.lib by the attached one I did so, now it works nearly fine. But now i have some problems with enabling some interupts. In the refe...
Posted on July 30, 2004 at 08:18Hi! > missing file... This is the decisive hint. Thanks a lot! Thanks for the mail with the complete project. I'll test ist later, my own project works fine now. Hein _b
Posted on July 28, 2004 at 13:49 Hi! sorry, i've seen it too late that there are 2 files to install. I've changed the CPDIV to CPUDIV and changed ''flagftatus'' to'' flagstatus'' in 71x_type.h Compilation is ok now, but i'm still in...