cancel
Showing results for 
Search instead for 
Did you mean: 

Timer Problem

adib
Associate II
Posted on March 15, 2004 at 10:51

Timer Problem

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
adib
Associate II
Posted on March 11, 2004 at 09:34

I'm working with the ST72264G u-C.

I'm using Timer A in ''one pulse mode'', and I want to use Timer B as ''output compare'' to indicate when a period of time has elapsed without output pin. (just to get interrupt when a period has elapsed).

In my application I want Timer B to be stopped until I enable it wait for the output compare interrupt and disable it back.

Since Timer B is free running, when I enable the interrupts using ''rim'' I get a timer B interrupt although I already set the TIMD bit in the CSR (and preformed a read from the CSR/OCBLR to clear the OCF bit).

Can anyone advise how the get rid from the first unwanted interrupt?

jatin
Associate II
Posted on March 15, 2004 at 08:56

It is not the normal behaviour. Could you attach your code ?

adib
Associate II
Posted on March 15, 2004 at 10:51

I suspected that I worked with a faulty chip.

I replaced it and everything is working.

Thanks