Posted on December 13, 2006 at 04:01Hi, I'm working with the ST72F264 micro. In my application I need to transmit a byte via the SCI and enable/disable external RS-422 driver. In order to disable the external driver I use the TC interrupt to know wh...
Posted on August 16, 2006 at 15:31Hi WoRo, I am aware of the that, actually I increment an image of the OC1HR/OC1LR counter and just before exiting the interrupt routine I load the image register into the OC1R with the correct order HB than LB. I no...
Posted on August 16, 2006 at 09:13Hi, I am working with ST72F264G2 mcu. I'm using timer A to generate PWM. In my application I need the PW to change from min to max progressively so I enabled timer A interrupt each time OCR1 (timer reset) happens. I...
Posted on July 14, 2006 at 12:27Hi, I'm working with ST72F264 micro. In my application PA0, PA1 are used as outputs connected to transistors. When I burn the micro everything works ok but when I try to debug using InDART-STX I get ''communication er...