2008-07-09 11:31 PM
2008-07-09 5:03 AM
Dear All,
I'm new stakeholder of ST devices. I'm using an STR750 with its Evaluation Board and CrossWork. I tried some Examples to use the LCD, UART, GPIO and I didn't find big difficulties. I'm now trying to use the examples related to TIM and Interrupt: void main() { #ifdef DEBUG debug(); #endif /* MRCC Configuration */ MRCC_Configuration(); /* GPIO Configuration */ GPIO_Configuration(); /* EIC Configuration */ EIC_Configuration(); /* TIM Configuration in Output Compare Toggle Mode ----------*/ /* CK_TIM = 60 MHz, Prescaler = 0x0, TIM0_CLK = CK_TIM/(Prescaler + 1) = 60 MHz */ /* OC1 update rate = TIM0_CLK / TIM_Pulse1 = 60 MHz/ 15000 = 4000 Hz (250 us) */ /* OC2 update rate = TIM0_CLK / TIM_Pulse2 = 60 MHz/ 6000 = 10000 Hz (100 us) */ /* TIM0 Channel1 configuration */ TIM_InitStructure.TIM_Mode = TIM_Mode_OCToggle; TIM_InitStructure.TIM_Prescaler = 0x0; TIM_InitStructure.TIM_ClockSource = TIM_ClockSource_Internal; TIM_InitStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_InitStructure.TIM_Period = 0xFFFF; TIM_InitStructure.TIM_Channel = TIM_Channel_1; TIM_InitStructure.TIM_Pulse1 = OC1Value; TIM_InitStructure.TIM_Polarity1 = TIM_Polarity1_Low; TIM_Init(TIM0, &TIM_InitStructure); /* TIM0 Channel2 configuration */ TIM_InitStructure.TIM_Channel = TIM_Channel_2; TIM_InitStructure.TIM_Pulse2 = OC2Value; TIM_Init(TIM0, &TIM_InitStructure); /* Preload register on TIM0_OCR1 and TIM0_OCR2 disabled: TIM0_OCR1 and TIM0_OCR2 values are taken in account immediately */ TIM_PreloadConfig(TIM0, TIM_Channel_ALL, DISABLE); /* Clear TIM0 flags */ TIM_ClearFlag(TIM0, TIM_FLAG_OC1 | TIM_FLAG_OC2| TIM_FLAG_Update); /* Enable TIM0 Output Compare1&2 interrupt */ TIM_ITConfig(TIM0, TIM_IT_OC1 | TIM_IT_OC2, ENABLE); /* Enable TIM0 counter */ TIM_Cmd(TIM0, ENABLE); while(1); } The example compiles fine but I was not able to realize how to verify the Interrupt on these lines. I tried to use the function EIC_GetCurrentIRQChannel() inside the loop: while(1){ if (EIC_GetCurrentIRQChannel()==TIM0_OC2_IRQChannel) ... } But this cause an incorrect verify of the Software downloaded in the Chip; is it correct to use the function EIC_GetCurrentIRQChannel() to verify the appear of the interrupt on a certain line, or I completly missunderstood the interrupt working way ?? Thanks a lot for any helps, regards LT [ This message was edited by: lnt on 09-07-2008 17:34 ]2008-07-09 11:31 PM
I tried to find out the problem,
I realized that in mine str75x_startup.s probably there is not a correct link to the irq_handler. It is written only: irq_handler: b. //endless loop Shall I add some System file?? or write something instead of this b. thank you in advance