Posted on May 17, 2011 at 12:38Dears, I'm trying to use crosswork like you, I found a problem with one function included in usb_istr.c, it is CTR_LP(), this function is not defined in any of the library I have. Someone have an idea about this ?? tha...
Posted on July 10, 2008 at 08:31I tried to find out the problem, I realized that in mine str75x_startup.s probably there is not a correct link to the irq_handler. It is written only: irq_handler: b. //endless loop Shall I add some System file?? or ...
Posted on July 09, 2008 at 14:03Dear All, I'm new stakeholder of ST devices. I'm using an STR750 with its Evaluation Board and CrossWork. I tried some Examples to use the LCD, UART, GPIO and I didn't find big difficulties. I'm now trying to use the ...
Posted on January 05, 2008 at 07:34I have a problem with the Joystick Mouse demo example for the STR750-EVAl Board. It' all ok if I use it with the IAR software, but it doesnt work if I create a new project with all files in Crossworks 1.7. Does any...
Posted on October 26, 2007 at 05:18I work with STR750-EVAL Evaluation Board and Crossworks 1.7. I have problem with the Joystick example downloaded from ST. The code loop forever at line while (pInfo->Current_Configuration == 0) NOP_Process(); I hav...