2013-01-31 9:02 PM
Hello,
I'm having a problem interfacing my ST7580 using Arduino Mega USART. And I think I already broke 2 pcs of IC and I cannot afford to lose some more.Please help me code to PING, Read/Write MIB and send even simple PHY data over the powerline.The Arduino code I used is here..../* Arduino Code � ST7580 Transceiver BoardCode Consideration: Not sure if syntax and arguments in User Manual work with all types of microcontroller. Just to be sure, per byte transmission will be used. For fields with >1 byte, endianness is assumed to start with byte index 0, which is the logical thing to do.Code Author: Patth Rick L. Ramirez, BS ECE 2008-11684*///GPIO Pin Assignments&sharpdefine aT_REQ 2&sharpdefine aBR0 3&sharpdefine aBR1 4&sharpdefine aPL_TX_ON 22&sharpdefine aPL_RX_ON 24&sharpdefine aPLC_RESETN 26//Local UART/Serial Pin Assignments&sharpdefine uC_TX 14 //RxD of ST7580 ; USART TX3 &sharpdefine uC_RX 15 //TxD of ST7580 ; USART RX3 //Analog Pin Assignments//&sharpdefine aCL_ADC 12 //hardware available but may not be necessary//&sharpdefine aPA_ADC 13/*Initialize variables*/ int avail = 0; byte inBUF = 0x00; //general purpose byte storage word inSTAT = 0x0000; //status message 2 bytes, index 0 should always be 3Fh byte inSTX = 0x00; byte inLEN = 0x00; // byte length of data field byte inCC= 0x00; byte inCSUM_LSB = 0x00; //checksum field is sent LSByte first byte inCSUM_MSB = 0x00; byte inDATA_0 = 0x00; byte inDATA_1 = 0x00; byte inDATA_2 = 0x00; byte inDATA_3 = 0x00; byte inDATA_4 = 0x00; byte inDATA_5 = 0x00; byte inDATA_6 = 0x00; byte inDATA_7 = 0x00; byte inDATA_8 = 0x00; byte inDATA_9 = 0x00; byte inDATA_10 = 0x00; byte inDATA_11 = 0x00; byte inDATA_12 = 0x00; byte inDATA_13 = 0x00; byte inDATA_14 = 0x00; //max number of data bytes as set by user == 16 byte inDATA_15 = 0x00;void GPIO_Init(void){/*Inputs*/ pinMode(aPL_TX_ON,INPUT); pinMode(aPL_RX_ON,INPUT); pinMode(aPLC_RESETN,INPUT);/*Outputs*/ pinMode(aT_REQ,OUTPUT); pinMode(aBR0,OUTPUT); pinMode(aBR1,OUTPUT);/*Initial Values*/ digitalWrite(aBR0,LOW); //set ST7580�s UART Baud rate to 9600 digitalWrite(aBR1,LOW); digitalWrite(aT_REQ,HIGH); //set to LOW if requesting transmission to ST7580} //GPIO_Init();void send_START(byte outSTX, byte outLEN, byte outCC){ Serial3.write(outSTX); Serial.println(''STX field is sent.''); digitalWrite(aT_REQ, HIGH); //bring back to default HIGH as soon as STX byte is received by ST7580 Serial3.write(outLEN); //byte length of data field Serial3.write(outCC);}//e.g. send_START(0x02, 0x05, 0x2C); void send_PING_DATA(byte PDATA){ Serial.println(''Pinging the ST7580 device...''); Serial3.write(PDATA); //make it a 3-byte data ping Serial3.write(PDATA); Serial3.write(PDATA);}//e.g. send_PING_DATA(0xAA); //CC for PingRequest is 2Chvoid send_CSUM(byte outCSUM_LSB, byte outCSUM_MSB){ Serial3.write(outCSUM_LSB); //checksum is sent LSB first Serial3.write(outCSUM_MSB); Serial.println(''Checksum bytes sent.'');}void setup(){ /*Initialize GPIO ports*/ GPIO_Init(); /*Set-up serial port 0 at 9600 bps � for printing data to the serial monitor*/ Serial.begin(9600); /*Initialize Serial Port 3 at 9600 bps, 8 data bits, 1 stop bit*/ Serial3.begin(9600); Serial.println(''Trying to PING ST7580 in''); Serial.println(''3...''); delay(1000); Serial.println(''2...''); delay(1000); Serial.println(''1...''); delay(1000); }void loop(){ delay(1000); while (Serial3.available() > 0){ inBUF = Serial3.read(); Serial.println(''Flushing FIRST.''); } //flush unnecessary receive buffer bytes do{ digitalWrite(aT_REQ, LOW); Serial.println(''Requesting transmission to ST7580.''); delay(150); inBUF = Serial3.read(); inSTAT = inBUF; delay(10); inBUF = Serial3.read(); inSTAT = inSTAT | (inBUF<<8); delay(10); Serial.println(inSTAT,HEX); if (inSTAT == 0x093F) Serial.println(''ST7580 is available.''); else Serial.println(''ST7580 is busy.''); } while (inSTAT != 0x093F); delay(30); //IMPT Why? send_START(0x02,0x06,0x2C); //PING Request send_PING_DATA(0xCB); send_CSUM(0x93,0x02); delay(30); //inBUF = Serial3.read(); // has stray FEh? while (Serial3.available() > 0){ inBUF = Serial3.read(); delay(50); Serial.println(inBUF,HEX); if ((inBUF==0x06) || (inBUF==0x15)) Serial.println(''Acknowledgement message received.''); else Serial.println(''Received what byte?''); } }//loop() Thank you very much to those who can help me. I hope you guys can I really need help. T_T #arduino #st75802015-04-29 10:03 AM
Hello,
I am working on st7570 using Ardunio UNO.But I can t find this c library(header and source code) everywhere.Maybe you can help me this issue.Regards,TOLGA