2003-07-22 2:18 AM
2003-07-21 11:58 PM
In the Datasheet of ST72324J/K the default Option Byte value is E7EF,
which means oscillator range (Option Byte 1: bit3,bit2,bit1) is set at value 111binary. According to the Datasheet this does not seem to correspond to any allowed bit combination. If I leave bit3 set, will my MCU still function without any problems or side-effects . Thanx in advance!2003-07-22 2:18 AM
Hello,
This is an error in documentation. STVP7 uses a default option byte value of E7E7 and will not allow you to change bit3 of option byte 1.