Posted on October 22, 2003 at 12:49Is it possible with the ST72F324 device to execute code in RAM between 100hex and 130hex assuming the Stack is empty i.e. pointing at 1FFhex.
Posted on August 26, 2003 at 06:58I'm developing flash driver software for ST10F168. My problem is that I can't program or erase the chip. I'm creating enough system stack (> 100 bytes), feeding R0,R1,R2,R3,R4 with the correct values and managing to...
Posted on July 22, 2003 at 08:58In the Datasheet of ST72324J/K the default Option Byte value is E7EF, which means oscillator range (Option Byte 1: bit3,bit2,bit1) is set at value 111binary. According to the Datasheet this does not seem to correspond...
Posted on June 11, 2003 at 08:47I'm trying to reprogramm a ST10F269-T6 device which is already mounted on a circuit. The St10 MCU is monitored by a L4969 device(system voltage regulator with a CAN Transceiver). I'm failing to get the MCU in Bootstra...
Posted on May 15, 2003 at 06:07I'm developing a Flash tool for St72F324(HDFlash). I'm doing the programming in ICP mode but once in a while when I execute the erase routine some areas of the Flash are left with the content 00hex although the status ...