2003-11-06 4:45 AM
2003-11-04 7:42 PM
Hi,
I'm looking for a ST7 chip with the maximum Baud rate (SCI) For RS232 communication - So far I saw only 500k - does any one know on any other chip with faster UART ? Thanks2003-11-05 7:30 PM
What i know is Maximum baud rate possible is 38.4 Kbps. Where have you found 500k?
2003-11-05 8:43 PM
Well....I'm working with the ST72321 and according to the Data Sheet you can reach 500k baud rate in the SCI.
2003-11-05 8:47 PM
500k is available will the following config @ 8MHz cpu:
TR & RR=1, PR=1 Regards sjo2003-11-06 3:16 AM
Hello
Can i get 1M or even more ? Latino2003-11-06 3:17 AM
I'm afraid as per the datasheet - 500k max for the sci
Regards sjo2003-11-06 3:23 AM
I've checked - According to the Data Sheet in my hands - using 16MHz osc can give you SCI with a 1M maximum.
Take a look on the Formula: Fcpu Tx = ------ 16 * ETPR*(PR*TR) Fcpu Rx =-------- 16 * ERPR*(PR*RR) So if ERPR=PR=RR = 1 and Fcpu=16Mhz => you can get 1M Baud Rate !!!! BUT !!! I've checked and tried it --- and you can't !!!! the Max is 500K [ This message was edited by: TeaMaker on 06-11-2003 16:54 ]2003-11-06 4:45 AM
Remember the maximum fcpu for the st7 is 8MHz not 16MHz.
Regards sjo