cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F276 debuging options

urik
Associate II
Posted on March 08, 2006 at 09:11

ST10F276 debuging options

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
urik
Associate II
Posted on March 08, 2006 at 08:36

Hello,

what are the software debugging options we have if we use the tasking compiler and the ST10F276?

are we bound to use the Rom-monitor (cross-view)?

if so can we put break points in the iFLASH and xFLASH?

if every thing else fails is there a recommended ICE to use?

thanks,

Uri.

najoua
Associate II
Posted on March 08, 2006 at 09:11

Hello Ukatry,

1/ what are the software debugging options we have if we use the tasking compiler and the ST10F276?

Please have a look to the enclosed AN provided by Tasking for details about debugging settings.

2/ Are we bound to use the Rom-monitor (cross-view)?

No, you are not bound to use the ROM monitor! You have the choice between RAM monitor(load your code in an external RAM) and ROM monitor(load your code in the flash).

3/ if so can we put break points in the iFLASH and xFLASH?

I am not sure that using Cross View to load code in the flash allows putting breakpoints. I will check this point and tell you.

4/if every thing else fails is there a recommended ICE to use?

You can use an ICE provided by Nohau. Please refer to the document available on the following link:

http://www.nohau.com/parts_lists/emst.pdf

Regards,

Najoua.

[ This message was edited by: Najoua on 08-03-2006 13:44 ]

[ This message was edited by: Najoua on 08-03-2006 13:46 ]

________________

Attachments :

TaskingAN.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0L6&d=%2Fa%2F0X0000000bXd%2FOVujbFTriLkwx6HaP2ocT6Ap8hhwFr25pCjj1vQYKEE&asPdf=false