cancel
Showing results for 
Search instead for 
Did you mean: 

Save the RTC with a battery

julienduay
Associate II
Posted on March 08, 2006 at 08:00

Save the RTC with a battery

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
julienduay
Associate II
Posted on March 08, 2006 at 07:26

Hello, I want to save the RTC on STR710 chip with a battery.

Can I save the RTC only by using the V18BKP pin?

Are RTCXTI and RTCXTO pins available if I use only the V18BKP pin?

Is the 3,3V mandatory to save the RTC?

Thank you :)

hichem2
Associate II
Posted on March 08, 2006 at 08:00

Hi,

For the RTC operation during Standby mode you will have to keep the 3.3V supply on the V33 pins even when you are using the 1.8V on V18BKP. In fact as described in the user manual, the 3.3V is necessary for powering the standby I/Os : (RTCXTI, RTCXTO, STANDBY and WAKEUP pin).

Hope that helps.

Hich

:o