2005-11-11 8:09 AM
2005-10-29 10:53 AM
Hiall!
I have an automotive board equipped with ST10F275. Is it possible to flash this MCU with the ST10Flasher V2.02B, and what is the difference between ST10F275 and 276?2005-10-31 9:28 PM
ohh thanxx for the info!
768KByte feprom and 36KByte ram :o now i understand why there is no external memory on this automotive control board. :) my other problem is, that i was unable to activate the bsl in the controller... i tied down pin D4 with a 1k resistor to ground, applyed a reset to the mcu but after sending 0x00 to the RXD0 i got no reply from the controller :-? [ This message was edited by: whoa on 01-11-2005 11:51 ]2005-11-11 8:09 AM
this pin on this panel is tied to ground with a 100nF capacitor and connected to vcc with a 220K resistor