2006-10-30 2:23 AM
RVDS 2.2 /Multi ICE with STR912FW44
2011-05-17 12:33 AM
Hello,
1/ Can somebody could provide me the necessary files to support an STR912 using a Full version of RVDS ? I think I just need .FME (Flash methods) and .BCD (board/chip definition). 2/ I see that tere is some specific register that permit to choose the order for the flashs. CAPS permit to porgram these. But are there any manner to access this using an arm program / or using RVDS ? Do I need buy a flashlink or rlink to manage this ? Sincerely Chris.2011-05-17 12:33 AM
Hi,
The number of documentations for STR9 is less than those for STR7. For STR7, we are able to find the files you need under ''Documents and files for family STR7/Software Patches/RVDK 2.1 (STR73xF)''. However, there is no file for the STR9 about this; it must be so moderators can help. Best Regards