2025-01-22 01:28 AM - last edited on 2025-01-22 01:31 AM by Andrew Neil
Hi ST Community,
I am using the board of STM32WBA55CGU6 board for OTA application and i want to use the application present in STM32Cube_FW_WBA_V1.3.0 and STM32Cube_FW_WBA_V1.2.0 packages. Since these packages are present in STM32Cube IDE version 1.15.0 and STM32Cube IDE version 1.14.0 respectively and is not available in the community for installation, i request to send the respective files to the mail id :- " shivaparbati2001@gmail.com "
Thank You.
2025-01-22 02:11 AM
Hello,
You can download older WBA packages there:
STM32Cube MCU Package for STM32WBA github
Select "Tags" instead of "Branches", choose the version and download zip.
2025-01-22 02:30 AM
Thank you
But i have the packages but i want the IDEs (stm32cubeIDE versions 1.14.0 and 1.15.0) as it is not available in ST Community. Please provide the IDEs files.
2025-01-22 02:34 AM
@Shaku Newer versions of STM32CubeIDE can work with older firmware versions, but not vice versa. You can and should therefore use the latest STM32CubeIDE and then install the desired firmware version.
Regards
/Peter
2025-01-22 02:41 AM
Thank You
After installing the newer version of the IDE the older version's packages are unable to select and unable to use and giving errors regarding errors after compilation.