2007-09-10 9:02 PM
2007-09-10 8:02 AM
Hi all,
I´m using ST72F63B microcontroller and after compilation the below messages are prompted: #error cpst7 io72263.h:7(14+4) redeclared localized PADR #error cpst7 io72263.h:9(14+5) redeclared localized PADDR #error cpst7 io72263.h:11(14+4) redeclared localized PBDR #error cpst7 io72263.h:13(14+5) redeclared localized PBDDR and so on... In actual fact, I´ve declared these variables once a time in io72263.h file as described below: volatile char PADR @0x00; /* Port A Data Register */ volatile char PADDR @0x01; /* Port A Data Direction */ volatile char PBDR @0x02; /* Port B Data Register */ volatile char PBDDR @0x03; /* Port B Data Direction */ volatile char PCDR @0x04; /* Port C Data Register */ volatile char PCDDR @0x05; /* Port C Data Direction */ volatile char PDDR @0x06; /* Port D Data Register */ volatile char PDDDR @0x07; /* Port D Data Direction */ and so on... Thus, I have no idea for these error messages. Where should I try harder in order to find out the problem? Thank you for any help, Wilson2007-09-10 9:02 PM
the message is quite clear: you declared every var more than once.
Maybe you include the same file twice, or you include a file with the declarations in a file where the vars are already declared: it should be easy to find out.