2011-11-10 6:52 AM
I would like to learn how to control the STR9 to create a reation timer program. When a button is pressed the unit waits a random time interval (between four and eight seconds) then begins incrementing LEDs on a bargraph display so that they appear to 'rise' upwards. When the user sees the LEDs moving, he presses a 'stop' button as soon as possible - the earlier the button is pressed, the fewer LEDs that are lit.
Can anyone show an example how to start with this?? Thanks #reaction #timer #divide-and-conquer2011-11-12 9:41 AM
If you can't solve a problem straight off, you need to break it down & down until you reach smaller sub-problems that you can solve.
This is the standard approach to any project; so best to start learning it now - rather than just ask for ready-made solutions. Think about the basic elements you're going to need:You should easily be able to find examples of these elements.
Note that an ARM9 is vastly overkill for this task - so your first simplifying step could be to start on a much simpler processor; eg, an STM8...2011-11-16 5:40 AM
Thnx andrew... As u mentioned , i divided thw hole task to start with a simple approach
1) Clear & Initialize LCD
2) Pressing and Initiating START button. 3) If the START Button is pressed, Start a timer count down. The counter should start at a random number and when it is reached, the LED have to start blinking in an incrementing way. ( 8 LEDs). This should continue moving back and forth as long as a STOP button is pressed. 3.1) The LED incrmenting should be also time dependant.abt 50ms between each LED step.4)When the stop button is pressed, It shows the delay in LCD
I will try to go through each step one by one2011-11-16 1:48 PM
I have a small question.
for (n = 0xFF; n != 0x00; n >>= 1) This line makes the LEDs to start from one corner (P7.0 to P7.7) in an increasing way. How do i adjust this LED blinking with a specified time interval.( random time )?? Also how do i intialize S2 and S3 for a specified task.? I couldnot find the initialization in anywhere.