2009-12-27 10:23 AM
2011-05-17 1:00 AM
Hi,
I’m trying to interface STR911FAW44X6 to a PSRAM device (MT45W4MW16BCGB). Unfortunately we’re using the LQFP128 package, which means we have to use some extra logic to get the correct interface. The problem I have at the moment is that EMI_WRHn and EMI_WRLn are pulled low during a read cycle! Is there a register I have to set to prevent this? We’re using Asynchronous mode only. The decode logic is: UBn = EMI_WRHn & EMI_RDn LBn = EMI_WRLn & EMI_RDn WEn = EMI_WRHn & EMI_WRLn Any help would be appreciated. Thanks, MM2011-05-17 1:00 AM
Hi mmgbmm
Strange behavior!!!! Could you please confirm that the default state of both EMI_WRHn & EMI_WRLn just after Reset is high ? Normally all EMI control signal are output high state after and during RESET. Cheers.2011-05-17 1:00 AM
Looks to me like misconfiguration of SCU_EMI register (LFBGA/LQFP), kinda like WRh/WRl work like UB/LB.
Try to change (see the register description in RM).