2004-07-12 5:32 AM
2011-05-17 3:02 AM
Installation of PSDsoft Express v7.90 on Windows 2000 makes that the system
hangs on boot. Before I had no problem under Windows NT4.0. Now I have to move to Windows 2000 (polish version). Effect is always the same, regardless of what other software is installed or what service packs and what patches are installed. In one of experiments PSDsoft Express was installed just after Windows itself and the system also hangs. Did anybody have such experience? And what to do?2011-05-17 3:02 AM
The latest version of PSDsoft is 8.10. Please download and use this version.
It can be found at:http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm
IMPORTANT: If you have a PC with HyperThreading or dual processors, be sure to see FAQ #109 at the following FAQ page:http://www.st.com/stonline/products/families/memories/psm/psdfaq.htm
2011-07-07 3:05 AM
Hello uPSD,
We are also struggling with PSDsoft Express version 7 , it simply hangs the PC during Programming PSD4235G2 Chip. As you had mentioned in your previous reply , We did try to download the Version 8.10 of PSD express . but unfortunetly its not on the Link mentioned below. So please can you send us the PSDsoft Express 8.10 version via e-mail tomailto:mandar.bagul@ge.com
This will be of great help. -Thanks & Regards- Mandar Bagul. Tech Lead. GE Oil & Gas Hyderabad, India. 91-40-402201872011-07-19 9:31 AM
Hi, the links that you posted are dead. Could you also send me a copy of PSDSoft express (latest version)?
mailto:jafrica@wms.com
Thanks2011-07-22 6:46 AM
Hello uPSD,
We are also developing with PSDsoft Express. We did try to download the Version 8.10 of PSD express . but unfortunetly its not on the Link mentioned below. So please can you send us the PSDsoft Express 8.10 version via e-mail tomailto:theo.spalinger@karlstorz.com