2005-02-24 10:08 PM
2011-05-17 3:05 AM
Hi all,
I got only a obj file(HEX format), and JCF file with uPSD 3233B. Can I get any PSD information from this Obj file? , such as ''Define PSD and MCU/DSP'', ''Pin/Node Functions'' ''Additional PSD Settings'' which defined in PSDExpress . Thank you very much.2011-05-17 3:05 AM
Thank you for reply!
Because I want to change the source and setting the PSD again, so I need to refer orgin PSD setting information. Do you have any suggestion to get the information from obj file, or other method? I am just a PSD beginner, need help.2011-05-17 3:06 AM
I mean that I don't have the ''ini'' which has original setting of PSD ,so I can not merge anything with HEX file, that is why I want to get that setting information from Obj file. I only have obj file, nothing else.
Thanks