2005-09-22 09:01 PM
programming the control register (st7538)
2005-04-27 11:35 PM
Hi Reny,
Sorry for my time response :( Please send me your email and then I send you my routine and we can talk about them. By.2005-05-04 07:30 AM
Hi flo123,
here is my e-mail address: reinhard_larch@yahoo.com.au thanks a lot, very much appriciated!!! Regards reny2005-05-11 09:55 PM
2005-06-09 04:42 PM
hi,flo123
Could you send me? my emial ismailto:yuanye-28@163.com
thank you very much.2005-09-20 01:55 AM
Hi,
I want to implement an FEC (forward error correction) in my ST7538 modem. What algorithm you had use ??? can you give me a suggestion :) Thank's2005-09-21 02:13 AM
Error Correction?
Well, I am using the old Hamming code. The amount of hamming bits to be used is up to you to decide... But there is a class of FEC codes called TURBO CODES that are much more efficient, but they need a lot of processing power. Rafael Krapf BRASIL2005-09-22 08:50 PM
Hi everybody,
I'm working with ST7538. I'm transmit between neutral fase and ground line to avoid problem in trifase system with 132,5 Khz frequency and 2400 baud. In some site I have problem of noise and the CD/PD line toggle. This problem occure some hours a day. By your esperience should I change some parameters as frequency or baud rate to improve the comunication ? I'm use a preamble byte every transmission to syncronize the comunication but during noise doesn't work correct. Have you suggest me a way to avoid noise by software ? What is the best configuration of register to avoid noise and have best performance ? Thanks to everybody help me....2005-09-22 09:01 PM
Hi Everybody,
another problem I have is a noise on clock CLR/T. In some device it's a stable but in other the clock swing. The hardware and components are the same. If I disconnect the transformer from line the clock became stable. Have you suggest something ? I have best performance with transformer 2:1. Thanks for help.