cancel
Showing results for 
Search instead for 
Did you mean: 

Programming/Erasing the internal Flash of 269

franz23
Associate
Posted on August 06, 2003 at 07:10

Programming/Erasing the internal Flash of 269

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
franz23
Associate
Posted on August 06, 2003 at 07:10

I'm using AN 1496 wich is confusing. Trying to erase the chip as it was described in table 1 don't work. I load the program in the internal ram and than I want to erase the whole chip. The Watchdog was turned on, because of the running program before. Is this a problem? Of course I have to service the watchdog also during erasing or programming the flash. I need correctly running program-samples in assembler whow erasing and programming is done, not like the confusing AN. Please help me.