cancel
Showing results for 
Search instead for 
Did you mean: 

More Than 2 12Bit PWM's ???

Posted on August 06, 2003 at 07:25

More Than 2 12Bit PWM's ???

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 05, 2003 at 12:09

Hello,

my problem is that I have to implement 3 12bit PWMs and one 10bit PWM inside the ST72321AR6! I knew that this device supports only 2 16bit PWM's and 4 8bit PWM's. Right?

But is it possible to expand the 4 outputs by using GP/IO's to a 10bit PWM? Or does anyone have a other idea?

Regards Andreas
sjo
Associate II
Posted on August 05, 2003 at 13:45

What frequency range are you after ?

Regards

SJO
Posted on August 06, 2003 at 07:25

I want to use the two 16 bit PWMs with the following configuration: 12bit with 1kHz.

Regards Andreas