2003-06-15 09:51 PM
program more chips with starter kit?
2003-06-15 06:31 PM
Dear Sir,
I want to know if I can use ST622XC-KIT (starter kit) to program st6200 or st6201 more than one chip simutaneously? Do I need make some change on the starter kit, for example, make a new adapter with two 16pin ZIF socket in parrellel, or can anyone provide some other way to implement to program more chips in one time? urgent! thanks. mcu interest2003-06-15 09:51 PM
Hi,
No - only one at a time. If you need this function, consider the MP8011A gang programmer from regards, Simon [ This message was edited by: sjh on 12-11-2003 16:25 ]