cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with Emulator

shermantec
Associate II
Posted on July 10, 2003 at 07:20

Problems with Emulator

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
shermantec
Associate II
Posted on May 17, 2011 at 11:34

I have e problem with ST9 emulator .I allwase get ''Connection error

(LPT1) st9+cannot enter monitor mode'' when I enter debug mode.I had this

problem befor but than when I reset the software and the emulator it start

workingcorrectly .Now It alwase stays with the same error after reseting

software and emulator.

Information about leds in the emulator:

After power is on all first three leds are on (Power,Emulator reset,ST9

reset).

After start debug mode , Emulator reset led turn off and after few seconds

'St9 reset' led turn off and Run led turn on and then I got the error.

why run led turn on ??

Please answare urgently

Regards

romain2399
Associate II
Posted on May 17, 2011 at 11:34

This error occurs when:

- the emulator probe is connected to an application board not power on, or

- the ST9 of the emulator probe, the ''emuchip'', is out of order. This can be caused by an emulator power off while the application board is power on.