2003-07-09 10:20 PM
2011-05-17 02:34 AM
I have e problem with ST9 emulator .I allwase get ''Connection error
(LPT1) st9+cannot enter monitor mode'' when I enter debug mode.I had this problem befor but than when I reset the software and the emulator it start workingcorrectly .Now It alwase stays with the same error after reseting software and emulator. Information about leds in the emulator: After power is on all first three leds are on (Power,Emulator reset,ST9 reset). After start debug mode , Emulator reset led turn off and after few seconds 'St9 reset' led turn off and Run led turn on and then I got the error. why run led turn on ?? Please answare urgently Regards2011-05-17 02:34 AM
This error occurs when:
- the emulator probe is connected to an application board not power on, or - the ST9 of the emulator probe, the ''emuchip'', is out of order. This can be caused by an emulator power off while the application board is power on.