2003-03-19 3:14 AM
2011-05-17 2:53 AM
I've drawn a card around the upsd3434a at 36 Mhz. I try first with a 12Mhz cristal with 2 capacitor (10pF) and it works well. It works well also with a 24Mhz cristal. But with a 36 Mhz there is no oscillation (I use also 10pF capacitors) ? Does I need to use a cristal resonator like on the DK3200 kit ?
Thanks, Sebastien2011-05-17 2:53 AM
Which voltage do you use?
2011-05-17 2:53 AM
I've find the problem, I've got a complete bottle of 36mhz cristal who doesn't work.
Thanks2011-05-17 2:53 AM
In fact there is an another problem with high speed quartz : current 36 Mhz cristal use the third overtone so it result a oscillation rate at one-third the desired speed so 12 Mhz. It's necessary to use a 36 Mhz cristal in is fundamental mode.