cancel
Showing results for 
Search instead for 
Did you mean: 

PSD 3200 XRAM space in von neumann mode

the_vice1304
Associate II
Posted on March 31, 2003 at 21:10

PSD 3200 XRAM space in von neumann mode

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
the_vice1304
Associate II
Posted on May 17, 2011 at 11:53

Hi guys,

is there a way to set the 8 KB internal XRAM space in Von Neumann mode ?

I would use it with keil's MON51 to test small programs (and not)

joseph2399
Associate II
Posted on May 17, 2011 at 11:53

Yes, the uPSD's SRAM can be setup using the Von Neumann architecture. When bit 0 of the VM register is set, _PSEN is used to access the SRAM as Program space. When this bit is cleared, _RD , is used to access the SRAM as DATA space. Please see page 117 of the uPSD323x data sheet for a graphical explaination.