2003-07-09 10:03 PM
2011-05-17 2:54 AM
Hi,
This is already given to you with PSDexpress. Firstly, go to Project > Preference and enable the ABEL equation editing capability. A new option will be given in the main design flow diagram - Edit / Add Logic statements When you enter this option, you will be shown the templates. Decoder 3-8 and Multiplexer 8-1 are in the General logic templates. Hope this helps Simon [ This message was edited by: sjh on 12-11-2003 16:26 ]2011-05-17 2:54 AM
With the PSDSoft Express I need to creat a multiplexer.
3 inputs ( PA6, PA5, PA4 ) and 1 output ( PB3 ). I want to control the multiplexer with an internal command. Does somebody have an idea how to easily realise this function with the internal PLD ? Br