Posted on May 17, 2011 at 11:55 I just startet to work with the DK3200 Development System. I loaded the ADC-sample application (AN1560) onto the system which works fine. But when I changed the flash memories in the PSDsoft Express tool (Pr...
Posted on May 17, 2011 at 11:54 With the PSDSoft Express I need to creat a multiplexer. 3 inputs ( PA6, PA5, PA4 ) and 1 output ( PB3 ). I want to control the multiplexer with an internal command. Does somebody have an idea how to easi...
Posted on April 27, 2004 at 07:22 Hi Hadi, If you look at the Ride Simulator manual, you will read that you can select between two kind of asembler : One from ST and one from Ride ... The one from Ride do not accept ''.window'' and ''....