Skip to main content
MKN
Associate II
October 7, 2024
Question

STUSB4761 - low level input voltage for I2C not compliante to spec?

  • October 7, 2024
  • 5 replies
  • 1167 views

Hi,
the maximum I2C input low voltage is stated as 0,35V for the STUSB4761.

Is this a typo?

Because in NXP I2C spec this level is stated as 0,3VDD 

We are using a PCA9516 I2C Multiplexer (0,5V Low) and observe massive connection failures with STUSB4761.

 

Regards

Michael

This topic has been closed for replies.

5 replies

TDK
October 7, 2024

Nothing would indicate it's a typo. 0.35 V is less than 0.3*VDD so is compatible with the NXP I2C spec.

> We are using a PCA9516 I2C Multiplexer (0,5V Low) and observe massive connection failures with STUSB4761.

Likely will need to debug this further. Look at the SDA/SCL signals on the line to see if they are valid or not. Ensure you have appropriate external pullups present.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MKN
MKNAuthor
Associate II
October 7, 2024

0.35 V is less than 0.3*VDD

That is the problem.
I2C Spec allows up to 1.5V for a valid Low_In (0.3*Vdd @ 5V )

STUSB fails if I2C low level is above 0.4V. (No ACK)
Furthermore it will detect a logical high above 1.2V.
1.2V is less than 1.5V.

Please explain how this could be compatible to NXP I2C spec.

 

I replaced the PCA9515 against a Nfet Switch / Level Shifter on SDA and the failure is gone.

TDK
October 7, 2024

> That is the problem.

You're right, I misread.

 

To the original question, it's unlikely to be a typo, especially as you've confirmed the issue. It appears this is done to prevent latch-up.

TDK_0-1728311872996.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
NBALL
ST Employee
November 27, 2024

Hello

Correct, please refer to table 16 for level triggering which need to be use. There is no typo .

Best regards

Nathalie