2003-08-05 10:25 PM
2003-08-05 3:09 AM
Hello,
my problem is that I have to implement 3 12bit PWMs and one 10bit PWM inside the ST72321AR6! I knew that this device supports only 2 16bit PWM's and 4 8bit PWM's. Right? But is it possible to expand the 4 outputs by using GP/IO's to a 10bit PWM? Or does anyone have a other idea? Regards Andreas2003-08-05 4:45 AM
What frequency range are you after ?
Regards SJO2003-08-05 10:25 PM
I want to use the two 16 bit PWMs with the following configuration: 12bit with 1kHz.
Regards Andreas