Skip to main content
itamar_nsu
Associate III
August 7, 2003
Question

inDart communication problem

  • August 7, 2003
  • 4 replies
  • 867 views
Posted on August 07, 2003 at 03:02

inDart communication problem

This topic has been closed for replies.

4 replies

itamar_nsu
Associate III
July 31, 2003
Posted on July 31, 2003 at 12:38

hi,

im a new user of the ST7LITE, the installation process of the application and the USB debuger went ok, and i have managed to run the asm sample program.

i dont know what went wrong, but now, when i try to run the program again i receive a ''communicatio error''. the inDart Diagnostic program is ok.. and i event tried to re-install the application. nothing works - is there any idea?
shreya
Visitor II
August 1, 2003
Posted on August 01, 2003 at 02:20

If you select ''Disable Option bytes'', put the jumper to provide clock to MCU from ICC connector and enter debug, do you still have the problem?

itamar_nsu
Associate III
August 1, 2003
Posted on August 01, 2003 at 05:26

No i dont - thanks!...

Do u know what was the problem?

[ This message was edited by: Itamar on 01-08-2003 09:31 ]

[ This message was edited by: Itamar on 01-08-2003 11:54 ]
shreya
Visitor II
August 7, 2003
Posted on August 07, 2003 at 03:02

The problem is because the device you used did not find the clock specified in its option bytes. So, you should select the ''Disable option bytes'' option in which case the device enters ICC mode without considering the option bytes programmed in it, but in this case it uses the external clock from the in-DART dongle board. The ICC jumper on the board connects this clock from the dongle (coming through the HE10 ICC connector) to the oscin clock of the device.