cancel
Showing results for 
Search instead for 
Did you mean: 

media for archival data doubt

ÍStef.1
Associate II

What media is good reliable for long term archiving data storage? SSD or HDD or MicroSD card or USB Flash Drive?

4 REPLIES 4
raptorhal2
Lead

Which device will be supported by something to read it when you need to?

My guess - USB Flash Drive.

 

ÍStef.1
Associate II

cold storage for backup data

Peter BENSCH
ST Employee

USB flash drives and SD cards contain the rest of the NAND flash production and are therefore only suitable for data transport, but not for data storage, especially not for long-term storage.

SSDs contain NAND flash with greater reliability than USB pen drives or SD cards, but they must be regularly connected to a computer so that the data can be refreshed.

Alongside optical data storage devices, hard drives are currently still the most suitable for long-term storage. However, they have the disadvantage that the interfaces used are slowly disappearing from the market (e.g. SCSI, PATA) and you have to keep such interfaces and possibly also the computers for them. However, the data can be copied to new devices when the interfaces are changed.

Summary: Long-term storage is a complex topic and should not be underestimated.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ÍStef.1
Associate II

Hard drives also have flash memory to store bios, firmware, smart files. Would this be a problem during long-term storage? If these files disappear from this flash memory, making the HDD unusable?

Is it a myth or a truth that HDDs are better for long-term storage of files without the need for power?