2007-01-02 9:21 PM
2011-05-17 12:30 AM
Hi
I cannot access my CPU with J-Link anymore after I did flash my own code into a str912-sk. Part of it write 0 into SCU->PRR0. J-Link stats it cannot stop the cpu. Is there a chance to do an ''full flash erase'' manualy ? Any help appreciate as I fear I otherwise killed the board :(2011-05-17 12:30 AM
Hi,
Try to use the CAPS tool in order to make an erase operation at least you can erase the Flash. pls find related documents through this link: http://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&fam=101#Software Regards Eris.2011-05-17 12:30 AM
I had the same problem. The only way I could erase the chip was to use a different debugger (ULINK from Keil). After the chip was erased, I could go back to the J-link (IAR) and continue hacking.
If you have the SEGGAR J-LinkFlash license, you can use this with IAR J-link to erase the chip.2011-05-17 12:30 AM
Hi,
CAPS tool supports now the Rlink jtag tool, you can us it instead of Flash link. Best regards, STARM2011-05-17 12:30 AM
I checked CAPS, but I for one have no parallel port anymore on my work-box and for the
other machine I have it runs Linux. Anyway thanks for the hint.