2006-10-25 9:37 PM
2006-10-25 3:42 AM
Hello,
I want to combine some assembly routines which handle my interrupts. First I have the IRQHandler which stores some registers onto the stack and calls my irq subroutine. next I have the irq subroutine which call two macros to switch between system and irq mode and calls the irq handler. This code works fine but I want to combine all the macros into the IRQHandler so I get one piece of assembly code. Is this possible and can someone give me that code since I don't understand asm code? Thanks p.s. attached you find the startup code and the irq handlers [ This message was edited by: s-wiggers on 25-10-2006 16:17 ] ________________ Attachments : irq.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJ4&d=%2Fa%2F0X0000000aLN%2FjphBDqOv44Yf9h020Fax10HsAIPo9rTVSxxD.iXxBLE&asPdf=falseStartup.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJ9&d=%2Fa%2F0X0000000aLO%2Fy6qQs402oCpgrXMPTLeCUs38.aKd7WkS_huG7q8AXvw&asPdf=false2006-10-25 7:57 AM
Here is how I handle interrupts. I modified interrupt handling code provided by ST. See if it makes any sense to you.
Regards, - mike ________________ Attachments : irq.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJE&d=%2Fa%2F0X0000000aLQ%2Fw6xATMKbEkthGKu_B7HPAxv2sWItjAqAqwpDAi4JRsY&asPdf=false2006-10-25 8:08 PM
Hello,
I see that you also have the ENABLE_IRQ() code in your irq handler. is it possible to put this code into the global irq_handler?? so I don't have to put it into every irq handler. Thanks.2006-10-25 9:37 PM
Yes, it can be done. You have to do it in the right order: read EIC_IVR first, then enable interrupts and call ISR. EIC initialization code would have to be modified too in order to accommodate a new way of calling ISRs via EIC_IVR.
The reason why I didn't do it is that interrupt handling code would inevitably become slower because of the manipulations with EIC_IVR. It kind of defeats the purpose of EIC_IVR, which is there to speed up interrupt handling. But if an extra microsecond or so in interrupt response time is not a problem, then what you are suggesting makes a lot of sense. I'll look into it when I have time. Regards, - mike