cancel
Showing results for 
Search instead for 
Did you mean: 

IOT solution

Jonamleonel
Associate II

A pattern is going to use P-NUCLEO-53L8A1 to monitor when a person get in to the bus , does anybody know how to send the information to the cloud via 4G or CAT and send GPS location, which devices should I use?

3 REPLIES 3
Peter BENSCH
ST Employee

You are not about a specific problem of the P-NUCLEO-53L8A1, but about a complete solution for sending the data including the GPS location via 4G/CAT. In addition to the ToF sensor, you need at least two other devices:

  • a GPS module (e.g. Teseo-LIV4F)
  • a 4G module (currently not available from STMicroelectronics)

You might consider the new low-power narrowband (NB-IoT) industrial module ST87M01 from STMicroelectronics, which also offers GNSS capability. The corresponding evaluation tool EVLST87M01 has already been announced and will hopefully be available soon.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@Peter BENSCH wrote:

You might consider the new low-power narrowband (NB-IoT) /Peter


@Jonamleonel mentioned this being on a bus - so, presumably, mobile ?

NB-IoT is not great for mobile applications!

LTE-M would be more suitable for a mobile application.

But these are both focussed on really power-constrained applications - which is probably not the case in a bus?

Andrew Neil
Evangelist III

The P-NUCLEO-53L8A1 is just a sensor evaluation kit:

https://www.st.com/en/ecosystems/p-nucleo-53l8a1.html

Sending data to the cloud really is an entirely separate issue - nothing to do with the sensors.

Data is just data - it makes no real difference where it came from.

There are dozens of different protocols that can be used to send data to the cloud:

https://www.google.com/search?q=microcontroller+send+data+to+cloud

 

If you want ST-specific material, try a search through the Knowledge Base; eg,

https://community.st.com/t5/forums/searchpage/tab/message?advanced=false&allow_punctuation=false&filter=includeTkbs&inactive=false&include_tkbs=true&q=iot