2009-09-24 7:24 PM
2011-05-17 12:57 AM
Hi all
I am not able to get clock on I2C clock out line I have done following configuration SCU_APBPeriphClockConfig(__I2C0,ENABLE); SCU_APBPeriphClockConfig(__GPIO2, ENABLE); SCU_APBPeriphReset(__I2C0, DISABLE); SCU_APBPeriphReset(__GPIO2, DISABLE); I2C_Cmd (I2C0, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 ; //GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; //GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; //GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; //GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO2, &GPIO_InitStructure); /* I2C0 Configuration */ //I2C_StructInit(&I2C_InitStructure); I2C_InitStructure.I2C_GeneralCall = I2C_GeneralCall_Disable; //I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_Ack = I2C_Ack_Disable; I2C_InitStructure.I2C_CLKSpeed = 400000; I2C_InitStructure.I2C_OwnAddress = 0xA0; I2C_Init(I2C0, &I2C_InitStructure); Uart0printf(''GO''); I2C_GenerateStart (I2C0, ENABLE); // Test on EV5 and clear it while( ! I2C_CheckEvent(I2C0, I2C_EVENT_MASTER_MODE_SELECT) ); Uart0printf(''Start1 Generated''); while(1) { //Uart0printf(''S''); I2C_SendData (I2C0, 0xAF); while (!I2C_GetFlagStatus (I2C0, I2C_FLAG_BUSY)); } OUTPUT: ''GOStart1 Generated'' Displayed on UART. Clock not received( Observed on CRO ) on I2C ClockOut when data byte is sent Is there any mistake in code written by me,please let me know. Regards Sai [ This message was edited by: sr_shinde on 05-03-2009 04:51 ]2011-05-17 12:58 AM
Sorry for late response.
I dont recollect the problem. But now I am using the same configuration and its working fine. I guess there was hardware problem. So please chech out with hardware ( I/O pins ). Regards Sai2011-05-17 12:58 AM
Have you solved the problem? I've got the same trouble!