Posted on May 17, 2011 at 09:59Forget about that, IT WORKS!! Many thanks... Why the f*** would we have to do that dummy read? Is it documented somewhere?
Posted on May 17, 2011 at 09:59Hi, I'm trying to use the secondary flash as an ''emulated eeprom'' like in the application note but it does not work, I get errors like ''FMI_TIME_OUT_ERROR''. Someone has tips to access Bank1 and write some bytes to ...
Posted on May 17, 2011 at 09:36Quote:On 01-02-2007 at 14:23, k7g2lm3 wrote: Hello, is there anybody who managed to have I2C working properly and could help me? My problem is that only start and stop bit work, but no address or data is sent over the...