2007-04-10 7:42 AM
2011-05-17 12:41 AM
I failed when trying to correlate and decode the various bits of
information concerning the GPIO port pins. Sources: REF: STR91xF reference manual. DS: STR91xF datasheet. PL: ARM PrimeCell PL061 documentation. Infobits: I1: According to DS 4.1, pin state can always be read as input. I2: PL suggests, that data read always reflects the PrimeCell input even when programmed as output. I3: According to REF 3.3 figure 22, the GPIO read logic receives 0 for all pins programmed as output. I4: According to REF 3.4.1, the GPIO data register reads the last value written to, for pins programmed as output. Questions: Q1: Is it true, that (I1) only holds for pins programmed as input? Q2: REF 3.3. figure 22 lacks information on which bits are used to enable the pin driver. There are 2 possible sources: the direction control of the PrimeCell (GPIO_DIR) and and the pin function control of the SCU (SCU_GPIOOUT). The figure shows a driver which is only controlled by SCU_GPIOTYPE, not by GPIO_DIR or GPIOOUT. Q3: IMHO (I2), (I3) and (I4) cannot all be true, if the ''GPIO read logic'' block in REF 3.3. figure 22 reflects the PrimeCell. So what is really read for pins programmed as output? The last state written to it, the state of the pins or 0? The pin state need not be idential to the output register state, if the output is programmed as ''open collector''. Q4: If the answer to Q3 is not ''pin state'', then how is it possible to connect a pin to a bidirectional open collector bus (such as used by Dallas 1-Wire devices)? How can it be avoided to explicitly switch the pin direction twice for each bit received? Background: Depending on the system environment, it may be necessary to mask interrupts for each GPIO_DIR or SCU read/modify/write sequence. [ This message was edited by: prx on 10-04-2007 20:13 ]