2006-10-17 11:59 PM
2006-10-02 2:37 AM
Hi all,
I am working on a instument that is indicating the analog value that is read in via the 12 bits ADC. The indicator is an analog pointer like an old voltmeter. I am looking for a filter to filter out small fast changes in the analoge input signal. The small slow changes must not be stopped by this filter. Also this filter may not generate a delay bigger than 0.5 sec. I tried avaraging multiple samples and I also implemented a first order filter. But or this filters delayed the input signal to much or they outputted results that let the analog pointer look like an digital one. Does someone have an effective filter(or idea's/tip's) or a good idea for me? Thanks Jimmey2006-10-02 4:48 AM
Hello.
And what analog RC filter? Did you really need sw solution? So... what is your sample rate? And what does it mean ''small fast change''? And how many instruction cycles do you have available for cumputing?2006-10-02 4:57 AM
Here is an extremely simple filter I use all the time:
#define FILTER_DEPTH 4 int filtered; void adc_conversion_done() { filtered += ADC_DATA - (filtered >> FILTER_DEPTH); } int adc_get_filtered_data() { return filtered >> FILTER_DEPTH; } It works similarly to an RC network with a time constant of (1 << FILTER_DEPTH) ADC sample times. Do the math and you will see why. Regards, - mike [ This message was edited by: volius on 02-10-2006 17:29 ]2006-10-04 3:57 AM
Hi mike,
Thanks, I had to increase the filter depth but it works fine now! Regards, Jimmey2006-10-17 9:33 PM
HELLO THERE...
CAN SOMEBODY PLEASE TELL ME THE ACCURACY OF THE ADC OF STR710FZ26.OR HOW TO CALCULATE IT.. KINDLY HELP REGARDS SANY2006-10-17 11:59 PM
Hi,
For the STR710 ADC12 converter, 1lsb = 3.3v/4095 = 2.5v/3103. With regards, Hich